Technical FAQs

Ask a Question

What should be selected on Lightning/Surge Arrester size question in the medium volatge metal enclosed product selector?<br />

It is best to let the Selector calculate the size based on the System Voltage and System Grounding. The Lightning/Surge Arrester Manufacturer has supplied this information.



CTA-ID : 2015659
Was this helpful?
What can we do to improve the information ?