Technical FAQs

Ask a Question

What is the dissipated power in watts for the ATS48D88Y soft starter for calulating heat loss?

The power dissipation in watts with the shorting / bypass contactor is 25W and without the shorting / bypass contactor is is 290W.

The the associated literature for additional details regarding mounting this product in an enclosure.


CTA-ID : 2015653
Was this helpful?
What can we do to improve the information ?