Technical FAQs

Ask a Question

What are the repair parts for the HU364A, series F6? (may be shown as F06)

Issue:
The list of repair parts is needed for Safety Switch catalog number HU364A, series F6.

Product Line:
Heavy Duty Safety Switch

Environment:
Applicable only to HU364A, Series F6

Cause:
The repair parts numbers for the HU364A, series F6, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable.

Resolution:
The repair parts for the HU364A, series F6 (F06) are as follows. No other parts are available.
-Complete Line/Load Base (all one piece) - 4056703950 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line/Load Base mounting screws - 40205-464-01 (requires 6 per line base)
-Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
-Arc Suppressor mounting screw - 40205-145-01
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 21401-222-40 (per lug)
-Switch Mechanism - 40566-786-50 (also requires Interlock Shaft Gasket 40567-860-01)
-Switch Mechanism mounting screws- 22999-405-62 (requires 2)
-Handle Assembly - 40566-635-50 (requires handle gasket 40566-031-01)
-Lockplate - 40566-721-01
-Lockplate mounting screws - 22999-405-62 (requires 2)
Was this helpful?
What can we do to improve the information ?