Technical FAQs

Ask a Question

What are the repair parts for the H464AWK, series F6? (may be shown as F06)

The repair parts for the H464AWK, series F6 (F06) are as follows. No other parts are available.
-Complete Line Base - 4056703650 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 40205-464-01 (requires 12 per line base)
-Load Base Assembly - 40566-774-50 (requires one per phase - includes phynolic base, lugs and fuse clips)
-Load Base mounting screws - 40205-464-01 (requires 2 per load base)
-Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
-Arc Suppressor mounting screw - 40205-145-01
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 21401-222-40 (per lug)
-Switch Mechanism - 40567-401-50 (also requires Interlock Shaft Gasket 40567-860-01)
-Switch Mechanism mounting screws- 22999-405-62 (requires 2)
-Handle Assembly - 40567-468-50 (requires handle gasket 40566-031-01)
-Lockplate - 40567-467-01
-Lockplate mounting screws - 22999-405-62 (requires 2)


CTA-ID : 2015391
Was this helpful?
What can we do to improve the information ?