Technical FAQs

Ask a Question

What is the 8536SBO2S2 starter?

This is a special starter for the 8941 Duplex controller. It consist of the basic 8536SBO2 starter but is supplied without control wiring and includes 1 (9999SX9) normally open early make external auxiliary contact mounted on the left hand top, 2 normally open (9999SX6) external contacts with 1 mounted on left hand bottom and the other mounted on the right hand top, and 1 (9999SX12) normally closed internal auxiliary contact mounted in right hand bottom internal slot.

CTA-ID : 2015637
Was this helpful?
What can we do to improve the information ?