Technical FAQs

Ask a Question

Is there a 45 degree lever arm available for the Class 9007 limit switches?

There is no fixed 45 degree lever arm for the 9007`s. However, the 9007AA1M, BA1M, CA1M, or DA1M can be adjusted to a 45 degree position.


CTA-ID : 2015370
Was this helpful?
What can we do to improve the information ?