Technical FAQs

Ask a Question

Are Square D buck-boost transformers rated for use indoor and/or outdoor?

Issue:
Buck and Boost Transformers are suitable for both indoor and outdoor use
 
Product Line:
LV Transformers
 
Environment:
Applies to all SquareD/Schneider Electric Buck and Boost Transformers
 
Cause:
Clarification of the Environment and NEMA enclosure rating for SquareD/Schneider Electric Buck and Boost Transformers
 
Resolution:
Yes. All Square D encapsulated transformers in inclosure styles __A, __B, or __C are NEMA 3R rated, which is suitable for both indoor and outdoor installations.


CTA-ID : 2015629
Was this helpful?
What can we do to improve the information ?