Technical FAQs

Ask a Question

How do I select a Back to Back line selector switch in the medium voltage metal enclosed product selector?

Issue:
How do I select a Back to Back line selector switch in the medium voltage metal enclosed product selector?

Product Line:
Metal enclosed switchgear.

Environment:
Products sold in the United States.

Cause:
Selection.

Resolution:
The Back to Back line selector is NOT available in N3R outdoor construction. Add the Main switch first, before the Line Selector Switch. Add the main switch from the Device drop down menu. Choose Main as the ``Switch Application``. Then choose the Lineside Connection for this Main switch as ``Back to Back Line Selector.`` Line selector switches are 600A & 1200A, 25kA & 38KA SYM short time current. 50kA SYM is not available. Line selector switches are non-loadbreak devices and have no arc chutes.




CTA-ID : 2015626
Was this helpful?
What can we do to improve the information ?