Technical FAQs

Ask a Question

How do I select a Side-by-Side line selector switch in the medium voltage metal enclosed product selector?

Issue:
How do I select a Side-by-Side line selector switch in the medium voltage metal enclosed product selector?

Product Line:
Metal enclosed switchgear.

Environment:
Products sold in the United States.

Cause:
Selection.

Resolution:
Choose Side-by-Side Line Selector switch as the ``Switch Application`` from the drop down menu. Add another switch from Device - Interrupter. Choose the ``Switch Application`` for this switch as a Main. Choose the Lineside Connection as ``Side by Side Line Selector``. Line selector switches are 600A & 1200A, 25kA & 38KA SYM short time current. 50kA SYM is not available. Line selector switches are non-loadbreak devices and have no arc chutes.



CTA-ID : 2015624
Was this helpful?
What can we do to improve the information ?