Technical FAQs

Ask a Question

Will the AL800MA7 lugs fit an I-line MH frame breaker?

Yes they can be installed on the load side of an MA or MH I-line branch breaker.


CTA-ID : 2015507
Was this helpful?
What can we do to improve the information ?