Technical FAQs

Ask a Question

What are the repair parts for the HU464DS, series F6? (may be shown as F06)

The repair parts for the HU464DS, series F6 (F06) are as follows. No other parts are available.
-Complete Line/Load Base (all one piece) - 4056704250 - (requires one base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Complete Line/Load Base mounting screws - 4020514202 (requires 12 per base)
-Arc Suppressor Assembly - 4056677550 (requires one per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056740150 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4055699850
-Cover Interlock Defeat Coupling - 4056718850
-Switch Mechanism mounting screws- 2194918121 (requires 2)
-Handle Assembly - 4056736850 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056738901
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screws - 2194918121 (requires 2)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801


CTA-ID : 2015497
Was this helpful?
What can we do to improve the information ?