Technical FAQs

Ask a Question

What kind of knockouts are on the bottom of a 2601AG or AH type drum switch?

There are two 1/2`` conduit knockouts on the bottom plate of that switch.


CTA-ID : 2015860
Was this helpful?
What can we do to improve the information ?