Technical FAQs

Ask a Question

What is the tap configuration of a 75T12H or the T12 voltage configuration for transformers?

The transformer has a total of four taps to compensate for high or low input voltage. It has: (2) 2.5% below and (2) 2.5% above.


CTA-ID : 2015859
Was this helpful?
What can we do to improve the information ?