Technical FAQs

Ask a Question

What type of hubs should be used on an NF panel with a top fed Nema 4X stainless steel enclosure ?

Issue:
What type of hubs should be used  on an NF panel with a top fed Nema 4X stainless steel enclosure ?

Product Line:
Panelboards.

Environment:
Products sold in the United states.

Cause:
Product features.

Resolution:
We have no recommendations regarding the use or selection of hubs for the installation of panelboards. Standard practices should be followed to meet the circumstances.


CTA-ID : 2015855
Was this helpful?
What can we do to improve the information ?