Technical FAQs

Ask a Question

What are the HOME LINE bus bars plated with?

Issue:
What are the HOME LINE bus bars plated with?

Product Line:
Load Centers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The aluminum bus bars are underplate with 99% pure copper and then plated with Tin. The process is BONDAL CF (cyanide free zincate). The total thickness is .0002 inches.


CTA-ID : 2015617
Was this helpful?
What can we do to improve the information ?