Technical FAQs

Ask a Question

Are optional lugs avaialble for the 9422 disconnects or operation mechanisms that will terminate 3 conductors per phase?

There are no 3 barrel lug options on the 9422 product line.


CTA-ID : 2015304
Was this helpful?
What can we do to improve the information ?