Technical FAQs

Ask a Question

What are the repair parts for the H664AWK, series F6? (may be shown as F06)

Issue:  
Current Design repair parts

Product Line:
Heavy Duty Safety Switches

Environment:  
Repair parts

Cause:   
Maintenance. 

Resolution:  
The repair parts for the H664AWK, series F6 (F06) are as follows. No other parts are available.

-Complete Line Base - 4056704950 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
-Line Base mounting screws - 4020506501 (requires 12 per line base)
-Load Base Assembly - 4056677450 (requires one per phase - includes phynolic base, lugs and fuse clips)
-Load Base mounting screws - 4020506501 (requires 2 per load base)
-Arc Suppressor Assembly - 4056677550 (requires one per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056740150 (also requires Switch Mechanism Gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (requires 2)
-Handle Assembly - 4056746850 (also requires Handle Gasket 4056603101)
-Lockplate - 4056746701
-Lockplate mounting screws - 2299940562 (requires 2)
-Ground Lug - 4025101652 (two required)
-Ground Lug Mounting Screw - 4020514801


CTA-ID : 2015608
Was this helpful?
What can we do to improve the information ?