Technical FAQs

Ask a Question

Is an I-Line FA or FY 1 pole breaker available with an auxiliary switch accessory?

Issue:
Is an I-Line FA or FY 1 pole breaker available with an auxiliary switch accessory?

Product Line:
Circuit breakers.

Environment:
Products sold in the United States.

Cause:
Accessories.

Resolution:
An alarm switch is the only accesory available on 1 pole FA or FY breakers.
A two-2 pole breaker would be needed to add one more electrical accessory like a shunt trip, UVR, or aux. switch.


CTA-ID : 2015492

Was this helpful?
What can we do to improve the information ?