Technical FAQs

Ask a Question

Will a 9001 K85 fit in the 9001 SKY2 enclosure with a 9001 SKR1GH13 ?

Yes, the 9001 K85 will fit in the enclosure
9001 K85
This module can be added to standard 9001 Type K, KX, SK or T momentary push button operators. Contact blocks mounted behind this module (maximum of 2) will be held in the depressed position when the operator is operated once and released to their normal position when the operator is operated again. For a N.C. circuit, use a 9001 KA3 or the N.C. contact of a 9001KA1 or the N.C. contact of a
9001KA4. For a N.O. circuit, use the N.O. contact of a 9001KA4 or
9001KA6.


CTA-ID : 2015490
Was this helpful?
What can we do to improve the information ?