Technical FAQs

Ask a Question

Is the lever arm included with the L140 cable switches?<br /><br />

No, The lever arm is purchased separately:
KA = 1.5``
KO = 2.5``
KB = 3.0``


CTA-ID : 2035507
Was this helpful?
What can we do to improve the information ?