Technical FAQs

Ask a Question

Where are the date codes located on FAL breakers?

They are on the lower right corner of the faceplate 5 digit number the first two numbers are the year, the second two are the week of the year, the last is the day of the week. Example: 04021.

CTA-ID : 2015849
Was this helpful?
What can we do to improve the information ?