Technical FAQs

Ask a Question

Customer needs a QOB, 30a, 2p breaker that is rated for 25K AIC.

Use the QHB230 for a stand alone rating of 65K AIC@240v. The QOB230 can be used in series with a choice of several up stream breakers per Digest 173 page 8-2 when series ratings are allowed.


CTA-ID : 2015848
Was this helpful?
What can we do to improve the information ?