Technical FAQs

Ask a Question

What is the part number of the outside RED operating knob or handle on 9070SK Transformer Disconnects?

Issue:
Replacement operator for 9070SK Transformer Disconnects

Product Line:
LV Transformers

Environment:
Applies to 9070 Class Transformer Disconnects by SquareD/Schneider Electric

Cause:
9070SK Transformer Disconnects have replaceable handle hardware

Resolution:
The part number for the Switch Operator is KCF2YZ





CTA-ID : 2015834
Was this helpful?
What can we do to improve the information ?