Technical FAQs

Ask a Question

Are the Horn Bypass Kits as installed in EZMH type branch units rated for continuous duty?

No, Horn Bypass Kits are limited to temporary use only while the local Utility is conducting their preventative MAINTENANCE check.
Ekstrom Industries, Inc. manufactures a meter socket closing plate supplied with a set of jumpers that can be used for 200A maximum contunious duty applications where a Watt-hour Meter is not required. Ekstrom can be reached at PH#: 800-532-4332 or 248-477-0250.



CTA-ID : 2035467
Was this helpful?
What can we do to improve the information ?