Technical FAQs

Ask a Question

Customer wants to know what the AIC rating of the NXL circuit breaker is when placed in a NA1200AWK enclosure?

The AIC ratings are as follows:
65k @ 240V ac
50k @ 480V ac
42k @ 600V ac.
These ratings are also marked on the wiring diagram of the enclosure.


CTA-ID : 2015485
Was this helpful?
What can we do to improve the information ?