Technical FAQs

Ask a Question

What are the repair parts for the H364NDS, series F6 (may be shown as F06)?

Product Line:
Heavy Duty Safety Switch

Environment:
Applicable only to H364NDS, series F6.

Resolution:
The repair parts for the H364NDS, series F6 (F06) are as follows. No other parts are available:
-Complete Line Base -4056703450 (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020514202 (requires 6 per line base)
-Load Base Assembly - 4056677450 (requires one per phase - includes phynolic base, lugs and fuse clips)
-Load Base mounting screws - 4020514202 (requires 2 per load base)
-Arc Suppressor Assembly - 4056677550 (requires one per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (Note: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056718850
-Switch Mechanism mounting screws- 2194918121 (requires 2)
-Handle Assembly - 4056736850 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056738901(also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screws - 2194918121 (requires 2)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801
-Neutral Assembly - SN20A
-Neutral Bonding Screw - 4028356651


 
Was this helpful?
What can we do to improve the information ?