Technical FAQs

Ask a Question

What is the maximum amperage branch breaker that can be used in the SC1624M100S Series M01?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Branch breaker provisions

Cause:
Application

Resolution:
The maximum branch breaker this device will accept is 125amp, BUT ONLY one and MUST be installed in the very top position on the interior. The remaining positions are limited to a 100amp maximum. SEE THE WIRING DIAGRAM OF THE DEVICE.


 
Was this helpful?
What can we do to improve the information ?