Technical FAQs

Ask a Question

What would be the replacement panel for the old obsolete QON442LS400?

Issue:
What would be the replacement panel for the old obsolete QON442LS400?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker load centers and panelboards sold and supported in the USA.

Cause:
QON442LS400 Replacement.

Resolution:
Would need to use the current NQ panelboard design to meet the specific application.

















CTA-ID : 2015807
Was this helpful?
What can we do to improve the information ?