Technical FAQs

Ask a Question

What is the difference is between a AL1000MAT and AL1000MA lug?

AL1000MAT is the same as the AL1000MA, except for the 6-32 tap control wire hole on the lug


CTA-ID : 2015798
Was this helpful?
What can we do to improve the information ?