Technical FAQs

Ask a Question

What are the repair parts for the H664DS, series F6? (may be shown as F06)

The repair parts for the H664DS, series F6 (F06) are as follows. No other parts are available.
-Complete Line Base - 4056704950 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
-Line Base mounting screws - 4020514202 (requires 12 per line base)
-Load Base Assembly - 4056677450 (requires one per phase - includes phynolic base, lugs and fuse clips)
-Load Base mounting screws - 4020514202 (requires 2 per load base)
-Arc Suppressor Assembly - 4056677550 (requires one per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056740150 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Switch Mechanism mounting screws- 2194918121 (requires 2)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056718850
-Handle Assembly - 4056736850 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056738901 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screws - 2194918121 (requires 2)
-Ground Lug - 4025101851 (two required)
-Ground Lug Mounting Screw - 4020514801


CTA-ID : 2015603
Was this helpful?
What can we do to improve the information ?