Technical FAQs

Ask a Question

What are the repair parts for the HU662DS, series F6? (may be shown as F06)

The repair parts for the HU662DS, series F6 (F06) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)

-Line Base - one each of 4056792750 (left side base), 4056792650 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included)
-Line Base mounting screw - 4020515101 (3 for each line base)
-Arc Suppressor Assembly - 4056635550 (requires 1 for left side, and 1 for right side)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056681201 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101652 - (2 total required)
-Ground Lug Mounting Screw - 4020514801

CTA-ID : 2015463
Was this helpful?
What can we do to improve the information ?