Technical FAQs

Ask a Question

Will breaker be resettable after shunt tripped if shunt accessory has constant voltage applied?

The breaker can be reset, but will trip open again if attempt is made to close it. The voltage will have to be removed from the shunt trip before the breaker can be closed.


CTA-ID : 2015790
Was this helpful?
What can we do to improve the information ?