Technical FAQs

Ask a Question

How can the ATV28 unit be run at a set speed without a speed signal input?

Issue:   How can the ATV28 unit be run at a set speed without a speed signal input?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   
If a forward or reverse run signal is given to the drive using the logic inputs and no speed signal is present, the drive will run at the LSP (low speed) setting. The factory default low speed setting is 0 Hz. This setting can be changed while the drive is running.


 
Was this helpful?
What can we do to improve the information ?