Technical FAQs

Ask a Question

What is the difference between the reed and the triac output on the SG08003 and which one is more durable?

The reed type is moving contacts and should be used with dirty power where the triac may not perform as well. The triac is solid state and should be used where exposed to vibration where it would last longer electrically.

CTA-ID : 2015787
Was this helpful?
What can we do to improve the information ?