Technical FAQs

Ask a Question

What Class motor overload protection does the ATV28 drive has?

The 230 and 460 Volt ATV28 drives have Class 10 protection.
The 575 Volt ATV28 drives have class 20 protection.


CTA-ID : 2015783
Was this helpful?
What can we do to improve the information ?