Technical FAQs

Ask a Question

What is the interior mounting hardware bag assembly part number for a 400A or 600A NQOD interior?

The part number is 80110-805-50. This bag assembly contains the hardware required to mount the interior in the box, circuit numbers and instruction manuals.

Revised 3/10/04

CTA-ID : 2005822
Was this helpful?
What can we do to improve the information ?