Technical FAQs

Ask a Question

What material is the Main Horizontal Cross bus in The EZM Main Devices?

Issue:
Product design features

Product Line:
EZM Metering

Environment:
Bussing material

Cause:
Application

Resolution:
The Main horizontal cross bus material is Aluminum


CTA-ID : 2015771
Was this helpful?
What can we do to improve the information ?