Technical FAQs

Ask a Question

What does CL error code on VSDO7 indicate because do not identify it in the list of faults?

CL is a status indication which informs that the unit is operating in current limit.

The output current has exceeded the CURRENT LIMIT setting (Parameter 25) and the drive is reducing the output frequency to reduce the output current. If the drive remains in CURRENT LIMIT for too long, it can trip into a CURRENT OVERLOAD fault (PF).


CTA-ID : 2014906
Was this helpful?
What can we do to improve the information ?