Technical FAQs

Ask a Question

What is the amperage rating on a RM4Tmeasurement relay

Resistive   Maximum 5 amps UL and CSA Current Ratings

Inductive Rating NEMA/UL B300) Inductive
3600 VA Make Rating
360 VA Break Rating
5 A Carry


CTA-ID : 2015073
Was this helpful?
What can we do to improve the information ?