Technical FAQs

Ask a Question

What is Fuselogic and what can be returned by the product selector?

FuseLogic provides the customer a more definite indication of blown fuse than just the pop-up pins of the fuses. Choose FUSELOGIC is the user wants fuse tripping. Fuse tripping requires the SEM mechanism. FuseLogic is available up to 38kV only on HVL/cc switchgear. FuseLogic can provide auxiliary dry contacts for blown fuse indication without fuse tripping.

FuseLogic is NOT available on Visi/Vac Circuit Interrupters. FuseLogic is NOT available on duplex switches because there is only one set of fuses. FuseLogic is NOT available on 1200A Switches.


CTA-ID : 2015072
Was this helpful?
What can we do to improve the information ?