Technical FAQs

Ask a Question

If the SEM HVL mechansim is selected, what type fuses are available in the product selector?<br />

The HVL switch with the SEM mechanism is most often used in conjunction with Fuselogic fuse tripping, therefore the Square D current limiting fuse is the standard.
Other fuses can be used and can be tagged in after discussion with the Smyrna TAG group. They can be no fuse tripping with other fuses.


CTA-ID : 2015070
Was this helpful?
What can we do to improve the information ?