Technical FAQs

Ask a Question

What is the short circuit rating of the PBC style Powerbus?

14KA for the 100 amp busway and 22KA for the 225 amp busway. Both amperages have a short circuit rating of 200KA when connected in series with either a Class J or Class T fuse.

CTA-ID : 2015041
Was this helpful?
What can we do to improve the information ?