Technical FAQs

Ask a Question

Is a ground lug provided on all of the PowerBus225 plug-in units? Does the busway have a ground conductor?

Yes, all of the plug-in devices come standard with ground lugs installed. The busway devices come standard with a 50% integral ground conductor on all lengths.

CTA-ID : 2015029
Was this helpful?
What can we do to improve the information ?