Technical FAQs

Ask a Question

What is the part number for the touch-up paint on the 8839 CPD?

The only two colors we have:

RAL7032- tan, beige
PK49SP- ANSI 49 Gray

Most 18 Pulse would be in a bolt-together ANSI 49 color but there could be a beige one out there.

CTA-ID : 2014897
Was this helpful?
What can we do to improve the information ?