Technical FAQs

Ask a Question

How do I pick the quantity of key interlocks required in the product selector?<br />Are HVL/cc key locks different from the other products?<br />

The quantities of key interlocks are picked by the locking scheme in the drop down menu. If extra locks are required, add them in Special Pricing at $610 list each. Note $610 List is the current list as of 01/19/04. It is subject to change. Check the current list price of key locks in the pricing guide for the product.

The key interlocks which are mounted on the HVL/cc mechanism are much smaller than the standard key locks and must be ordered from Schneider Electric Canada. Also all locks that coordinate with these locks must be ordered with them.

CTA-ID : 2015273
Was this helpful?
What can we do to improve the information ?