Technical FAQs

Ask a Question

Customer asks if the 8430MPDV24 will function on a 208v system?

This can be adjusted down to 75% of the nominal voltage of 240 volts, or down to 180 volts. So it will work on 208 volts.

CTA-ID : 2015063
Was this helpful?
What can we do to improve the information ?