Technical FAQs

Ask a Question

Is there a NEMA 4X or Type 4X handle operator available for the D10S* disconnect switches?

No, the rotary handle operating mechanisms available are rated NEMA Type 1, 3, 3R, 4 and 12 only.

CTA-ID : 2015028
Was this helpful?
What can we do to improve the information ?