Technical FAQs

Ask a Question

What is the speed reference the unit runs at when have the various possible combinations of LI2, LI3 and LI4 set for 8 preset speeds on the ATV28 unit?

 LIz       LIy           LIx            Frequency Reference
 0           0              0      =          LSP ( low speed )
 0           0              1      =          SP2 ( preset speed 2 )
 0           1              0      =          SP3 ( preset speed 3 )
 0           1              1      =          SP4 ( preset speed 4 )
 1           0              0      =          SP5 ( preset speed 5 )
 1           0              1      =          SP6 ( preset speed 6 )
 1           1              0      =          SP7 ( preset speed 7 )
 1           1              1      =          HSP ( high speed )


CTA-ID : 2015022
Was this helpful?
What can we do to improve the information ?