Technical FAQs

Ask a Question

What the current specifications for the 24vdc internal supply on the ATV28?

Issue:   What the current specifications for the 24vdc internal supply on the ATV28?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Customer current available is 100mA.
The +24v is protected against short-circuits and overloads, min. 19v, max. 30 V. Max.


 
Was this helpful?
What can we do to improve the information ?