Technical FAQs

Ask a Question

What is meant by the error ``Must designate an Incoming Section`` in the Product Selector?<br />

If the lineup is all feeders, the selector must know which feeder section has the incoming power cables that tap on to the main bus. One of the feeders must have incoming cables rather than main bus.

CTA-ID : 2015254
Was this helpful?
What can we do to improve the information ?